Skip to main content
connected-resturants

The Connected Restaurant Program Delivers Big Gains for Restaurant Chains

The program has digitally transformed restaurant operations, enhanced guest comfort and reduced energy costs for Quick Service Restaurant chains.

The Connected Restaurant Program uses Internet of Things (IoT) edge devices, an Artificial Intelligence (AI) and IoT platform along with human expertise to enable restaurant operators to efficiently manage equipment operations. The service helps deliver quick positive cash-flows and can be scaled from a few hundred restaurants to thousands. The Abound Egde system offers edge connectivity and control, predictive actionable insights and autonomous actions by the Abound Insights platform and 24/7 remote support and proactive actions by the BluEdge™ Command Center.

The program enables restaurant operators to collect information from all connected devices like Heating, Ventilation and Air Conditioning (HVAC) systems, refrigerators, cooking equipment and lighting to effectively manage their facilities through predictive insights. Restaurant operators can easily monitor critical components such as air quality, temperature and humidity and help create a better indoor environment. The main aim of the program is to enable restaurant operators to digitally transform their operations - to make them more predictive and proactive. As of Q2 2021, this service is deployed globally across over 1,300 restaurants of multiple leading brands, saving over 44 million kWh, while improving maintenance processes, food safety and occupant comfort. Here is a quick glance of a few case studies, showing the results of using the connected restaurant program for the past 4 years or more.

Please fill out the form below to read the full case study.
 

The program enables restaurant operators to collect information from all connected devices such as Heating, Ventilation and Air Conditioning (HVAC) systems, refrigerators, cooking equipment and lighting to effectively manage their facilities through predictive insights. Restaurant operators can easily monitor critical components such as air quality, temperature and humidity and help create a better indoor environment. The main aim of the program is to enable restaurant operators to digitally transform their operations - to make them more predictive and proactive. As of December 2023, this service is deployed globally across over 2000 restaurants of multiple leading brands, saving over 93 million kWh across current and completed engagements, while improving maintenance processes, food safety and occupant comfort. Below are a few case studies, showing the results of using the Connected Restaurant Program as of December 2023.

Download the Case Study arrow_forward